Hi,
I have had a look into the HET IDE and also the TMS570LS31x documentation, but still some parts are a bit unclear to me.
1. Is the limit of 160 instructions stated per N2HET, i.e 160 instructions available for N2HET1 and 160 instructions available for N2HET2?
2. Are there any sigificant differences between the N2HET1 and N2HET2 modules except for amount of dedicated pins?
3. I have seen some encoder example code here on the forum. Are there any restrictions of how to use the HET pins? Can I choose any two of the HET pins to cooperate as an encoder?
4. Is the data field for each instruction accessable by an application running on the TMS570? Or is it so that the data has to be transferred to some specific registers in order to be accessable by an application?