Other Parts Discussed in Thread: CC3100
Hi,
I wanted to know if the board is compatible with the wifi module cc3000?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC3100
Hi,
I wanted to know if the board is compatible with the wifi module cc3000?
Thank you
miguel saldana said:wifi module cc3000
Do you mean the CC3000 Booster Pack EVM Board, or just the CC3000 Module?
Just by doing a quick comparison with the Pin connections of CC3000 booster pack to EK-TM4C129, CC3000 Booster Pack is compatible with Booster Pack 1 connector of EK-TM4C129,
See, also CC3100 Booster Pack.
- kel
Any cc3000 board.
like this one
http://www.adafruit.com/product/1469
or this one
http://www.digikey.com/product-detail/en/CC3000EM/296-35492-ND/3768419
thanks!!!!!
Hi, CC3000 support is provided on TIVAWare package, if you plan use boosterpack you can use near out of the box just setup network parameter.
If you plan use other board then also hardware connection of SPI and GPIO are required too, nothing so complex than wire up a few pin BP_TIVA to CC3000 Device.