Other Parts Discussed in Thread: RM46L430
Hi,
This is regarding the MibSPI/SPI timing details mentioned in the
RM46L430 datasheet..."5.11.4 MibSPI/SPI Master Mode I/O Timing Specifications"
The Table 5-32 (page 150) mentions about Parameters tr(SPC)M, tf(SPC)M, tf(SPICS), tf(SPICS)...
but there is no proper explanation of these parameters in the Figure 5-14.
1.Are these parameters related to Rise time and Fall time as shown in the below figure?
2.Can we assume tf(SPC)M & tf(SPC), tr(SPC)M & tr(SPC) are same parameters?
we are confused because there is no 'M' at the end of "tf(SPC)" parameter...
Could you please confirm if the above understanding is correct.
Best Regards
Prad