Hi,
I wonder if Texas has plans for TM4C129x with 0.5mm pitch in LQFP package. Or plans for another cortex-m4 serie with MAC or MAC + PHY in 100 pins 0.5mm LQFP package, so we can have compatible board design with a TM4C123xxxPZ for example.
Ari.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I wonder if Texas has plans for TM4C129x with 0.5mm pitch in LQFP package. Or plans for another cortex-m4 serie with MAC or MAC + PHY in 100 pins 0.5mm LQFP package, so we can have compatible board design with a TM4C123xxxPZ for example.
Ari.
Hello Ari,
As of now there are no plans to have a 100 pin QFP package with MAC or MAC+PHY. But will surely post an update it a new package or pin-compatible TM4C is on the anvil.
Regards
Amit