I can't get any of the FATfs examples to work with my TWC123GXL launchpad(s) and the SD Booster pack. I am using ccs version 6.0.1.00040
It petit FAT FS works fine on an MSP430-exp430g2 with the same launchpad and SD Card. Also the fatsd_StellarisLM4F232H5QD sample project worked fine with EKS-LM4F232 and the same micro SD Card (used an adapter for the SD Booster pack).
The SSI2 works well for robG's Touchscreen display.
Console output from fatsd_TivaTM4C123GH6PM is and fatsdraw_TivaTM4C123GH6PM was:
Starting the FatSD example
Drive 0 is mounted
Creating a new file "fat:0:input.txt"...Error: "fat:0:input.txt" could not be created
Aborting...
Starting the FatSD Raw example
System provider is set to SysMin. Halt the target and use ROV to view output.
Drive 0 is mounted
Creating a new file "0:input.txt"...Error: "0:input.txt" could not be created
Aborting...
I had similar results with several other examples.
I spent two days and would really appreciate any help
Michael Kadie