Other Parts Discussed in Thread: HALCOGEN
Hello,
I'm using RM48 development board with CCS 6 and HalCoGen.
The application hangs in checkRAMECC() after it inserts a double bit error, then tries to read it,
ramread = tcramA2bit;
Single stepping through the code, when I click to single step over this line, I see "No source available for "0x10" "
In the disassembly window, address 0x10 shows "Target failed to read 0x10 [ code = 0x1]"
When not single stepping, just running in debug mode, I see a similar message "No source available for "0x0c" "
In the disassembly window, address 0x0c shows "0000000c: DFFFFFFF SVCLE #16777215"
I'm lost as to what is causing this. Any assistance would be great!
Thanks,
Matt