Hi
I'm trying to port the FlexRay Example from the TMS570LS31 HDK to the TMS570LS12 HDK.
My setup consits of two HDK's which each have a FlexRay TJA1081 Phy. This two boards are directly connected with 2 short twisted wires.
On the RX/TX Pins of each controller i see that they receive the Message from the other Controller. Both controllers are the howl time sending Startup Messages. (Null Frame Indicator = 0, Sync Frame Indicator = 1, Startup Frame Indicator = 1) So it seems that they aren't able to finish the FlexRay startup.
Are there some differences between the LS31 and LS12 FlexRay Controller? Or have i made some stupid error? Any tips what i should change to get the startup finished?
Best regards
Fabian Page