Other Parts Discussed in Thread: TMS570LC4357
hi ti,
i m using TMS570LC4357
i have written a code to blink led and send ACK upon reception of corresponding commands.
led blink function is copied to sdram using emif and is called in sci isr.
if i simply receive a frame i can transmit ACK(sci txn works properly). but if i receive frame respective to
led blink function, the function is called correctly but after that i cant send ACK (sci txn is not working).
sci transmits the ACK only ater receiving another fame.(ie. txn happens when rx int is detected).
why this s happening? i need to send the ACK immediately after calling the func.
sci settings:
baud rate=115200; data bits=8; stop bits=1; enabled rx int and tx int; mode= address bit mode;
should i ve to enable some other settings??