Other Parts Discussed in Thread: EK-TM4C123GXL, EK-LM3S3748, LMFLASHPROGRAMMER, LM3S3748, LM3S2965
Hi,
I'm using CCS-5.4 foe EK-TM4C123GXL LauchPad.
I have an unstable condition in debugging the launchpad using CCS-5.4, more than 50% I have the error below and CCS gets hung
I tried with
1) Example "project0" and "hello" example from TivaWare for the board EK-TM4C123GXL
2) I tried with both CCS-5.4 and 5.5
3) Just click "DEBUG" and the error poped after a while, haven't got a chance to run it, then it got hung, the CCS appears DIM, unable to close
Below is the error msg
CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
CORTEX_M4_0: Error: Timed out while waiting for target powerup/polling a hardware resource.
Any idea would be appreciated
Thanks,
~Duy-Ky