Hi,
I'm able to get SPI (SSI in TI term) signal on pin header on the EK-TM4c123GXL.
However it signal is ONLY HALF of specs (1.5v vs 3.3v) when connected to SPI slave. The level is 3.3v when no connection.
I have a EK-LM3S2965 and checked the level is the same 3.3v when connected to the slave
I tried with max strength 8MA only to add 0.2v to get 1.7v
What's else I can do ?
Thanks,
~Duy-Ky