This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing RTC DS1307

Hi,

I want to interface RTC ds1307 with Tiva using I2C.I have gone through the working of I2c module in Tiva ,as it has been given in an example of Tiva codes.

I have interfaced the RTC module in PIC using register level programming ,but finding it difficult to implement in Tiva.

I am not getting any helpful code on forum which I could refer to.Along with that this new GUI of E2E is making the situation a bit more difficult...

  • Hello Kishore,

    It seems that the search system has failed on TM4C (unwanted side effect of the update). In the meantime can you please describe the issue, attach the code and scope/LA waveform of what you are seeing?

    Regards

    Amit

  • Hi,
    Following is my code, I have connected SCL to PB2 and SDA to PB3,along with that I have connected 4.7k pullup reistors with SCL and SDA .I am trying to print the output on my serial monitor through UART but I am not getting any response over there.Please help me debug my code!!!!

    • board-Tm4C123G Launchpad
    • crystal frequency-32.768 Khz




    #include "hw_memmap.h"
    #include "hw_types.h"
    #include "hw_i2c.h"
    #include "i2c.h"
    #include "sysctl.h"
    #include "gpio.h"
    #include "uartstdio.h"
    #include "systick.h"
    #include "uart.h"
    //#include "Debug1.h"
    #include "ustdlib.h"

    #define BYTE unsigned char
    #define SLAVE_ADDRESS 0x68
    extern void InitConsole(void);
    extern unsigned char dec2bcd(unsigned char val) ;
    extern unsigned char bcd2dec(unsigned char val) ;



    unsigned char dec2bcd(unsigned char val)
    {
    return ((val/0xA*0x10)+(val%0xA));
    }

    // convert BCD to binary
    unsigned char bcd2dec(unsigned char val)
    {
    return ((val/0x10*0xA)+(val%0x10));
    }
    void InitConsole(void)
    {

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    GPIOPinConfigure(GPIO_PA0_U0RX);
    GPIOPinConfigure(GPIO_PA1_U0TX);

    GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    UARTStdioInit(0);
    }

    int main()
    {
    unsigned long sec=3,min =59,hour = 12,day = 4,date = 3,month = 12,year = 10,tsec,tmin,thour,tday,tdate,tmonth,tyear;
    unsigned char Last_Value = 1;
    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_8MHZ);
    InitConsole();

    SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    SysTickPeriodSet(SysCtlClockGet());
    SysTickEnable();

    GPIOPinConfigure(GPIO_PB2_I2C0SCL);
    GPIOPinConfigure(GPIO_PB3_I2C0SDA);
    GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_2 | GPIO_PIN_3);

    I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet(), false);
    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS , false);

    I2CMasterDataPut(I2C0_MASTER_BASE, 0);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_START);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(sec));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(min));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(hour));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(day));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(date));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(month));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterDataPut(I2C0_MASTER_BASE, dec2bcd(year));
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    while(1)
    {
    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS , false);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_START);

    I2CMasterDataPut(I2C0_MASTER_BASE, 0x00);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS , true);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    sec = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    min = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    hour = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    day = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    date = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    month = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    year = I2CMasterDataGet(I2C0_MASTER_BASE);

    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
    while(I2CMasterBusy(I2C0_MASTER_BASE));

    tsec = bcd2dec(sec)&0x7f;
    tmin = bcd2dec(min);
    thour = bcd2dec(hour)&0x3f;
    tday = bcd2dec(day);
    tdate = bcd2dec(date);
    tmonth = bcd2dec(month);
    tyear = bcd2dec(year);
    if(Last_Value != tsec)
    {

    UARTprintf("%02d:%02d:%02d \n%02d %02d/%02d/%02d\n",thour,tmin,tsec,tday,tdate,tmonth,tyear);
    Last_Value = tsec;
    tsec = 0;
    }

    }


    }

  • Hi,
    Above mentioned is my code ,I am not able to get any response from the I2c rtc ds307.please do help me out in debugging my code?