Other Parts Discussed in Thread: HALCOGEN
I am using Halcogen and SPI1 in interrupt mode to communicate with an IMU (MPU6000). I am performing a SendData() several times and then performing a SendAndGet(). However, it seems to take the RXINTFLG a long time to be set. This results in my read actually reading the previous Rx data.
To explain, here is a segment of the HALCogen Tx buffer empty interrupt handler, where a dummy read is performed:
spiREG1->DAT1 = ((uint32)DataFormat << 24U) |
((uint32)ChipSelect << 16U) |
(WDelay) |
(Chip_Select_Hold) |
(uint32)Tx_Data;
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
g_spiPacket_t[0U].txdata_ptr++;
/* Dummy Receive read if no RX Interrupt enabled */
if(((spiREG1->INT0 & 0x0000FFFFU)& 0x0100U) == 0U)
{
if((spiREG1->FLG & 0x00000100U) == 0x00000100U)
{
SpiBuf = spiREG1->BUF;
}
}
The problem is that the Rx data comes too late and the RXINTFLG is set too late, and therefore this dummy read never occurs. Therefore, the next time I perform a Write and I enter this interrupt handler, instead of performing a dummy read of the current Rx data, I perform a read of the previous data (which has arrived by this time).
The final result of all this is that when I finally call SendAndGetData(), I go to the Rx interrupt before I get to the Tx interrupt because the RXINTFLG is still set from the Rx data of the last Write (because it was never read using the dummy read!).
The best way I see to take care of this is to clear any RXINTFLG before performing a SendAndGetData(). However, once again, it takes some time for the flag to be set, so I need to wait for the RXINTFLG to before I can clear it:
spiSendData(spiREG1, &imu_dataconfig, 2, txData);
while(SpiTxStatus(spiREG1) != SPI_COMPLETED);
// Wait for RXINTFLG to be set
while((spiREG1->FLG & 0x00000100U) != 0x00000100U);
// Clear the RXINTFLG
if((spiREG1->FLG & 0x00000100U) == 0x00000100U){
// Read the buffer to clear the flag
uint32_t spiBuf = spiREG1->BUF;
// In case there was data in RXBUF, clear the flag again
spiREG1->FLG = 0x00000100U;
}
txData[0] = (0xF5);
txData[1] = 0;
spiSendAndGetData(spiREG1, &imu_dataconfig, 2, txData, rxData);
This is fine with me. I would just like to know if there is any reason why it takes the Rx data and the RXINTFLG so long to be set? It seems to affect the functionality of the HALCogen code.