Other Parts Discussed in Thread: TMS570LS1224
Hi,
I have question about redundancy of nPORRST pin.
Now, I use the TMS570LS1224 and TPS65381.
These devices are connected by SPI pin and Reset(nPORRST & NRES) pin.
Please teach me the following.
When using this combination:
If the SPI terminal is damaged, reset signal is output to nPORRST(TMS570) from NRES(TPS65381) by QA watch dog.
This means that system can detect the error of the SPI terminals.
If the NRES terminal is damaged, TPS can't output reset signal.
This means that TMS570 can't detect the error of NRES terminals.
Is there a way TMS570 detects the error of NRES terminals.
Best regards,
FSSer