This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC interrupt of TimerA, no interrupt

I have been trying to get the ADC to be read at a timed interval. I have the interrupt working for timer A to where it is going into the interrupt. The ADC isn't going into any interrupt.

#include <stdint.h>
#include <stdbool.h>
#include <math.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "inc/hw_gpio.h"
#include "driverlib/fpu.h"
#define TARGET_IS_BLIZZARD_RB1
#include "driverlib/rom.h"

#define PWM_FREQUENCY 55


int main(void)
{
	volatile uint32_t ui32Load;
	volatile uint32_t ui32PWMClock;
	volatile uint8_t ui8Adjust;
	ui8Adjust = 83;

	uint32_t ui32Period;

	ROM_SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
	ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);

	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

	ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

	ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
	ui32Period = (ROM_SysCtlClockGet() / 10) / 2;
	ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, ui32Period -1);

	ROM_GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
	ROM_GPIOPinConfigure(GPIO_PD0_M1PWM0);

	ROM_ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_PROCESSOR, 0);
	ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_TS);
	ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_TS);
	ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_TS);

	ROM_ADCSequenceStepConfigure(ADC0_BASE,1,3,ADC_CTL_CH0|ADC_CTL_IE|ADC_CTL_END);

	ROM_ADCSequenceEnable(ADC0_BASE, 1);

	HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
	HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
	ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
	ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);

	ui32PWMClock = SysCtlClockGet() / 64;
	ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
	ROM_PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
	ROM_PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, ui32Load);

	ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
	ROM_PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT, true);
	ROM_PWMGenEnable(PWM1_BASE, PWM_GEN_0);

	ROM_IntEnable(INT_TIMER0A);
	ROM_IntEnable(INT_ADC0SS1);
	ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
	ROM_TimerEnable(TIMER0_BASE, TIMER_A);

	ROM_IntMasterEnable();





	while(1)
	{

		if(ROM_GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_4)==0x00)
		{
			ui8Adjust--;
			if (ui8Adjust < 36) //56
			{
				ui8Adjust = 36;
			}
			ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
		}

		if(ROM_GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_0)==0x00)
		{
			ui8Adjust++;
			if (ui8Adjust > 128) //111
			{
				ui8Adjust = 128;
			}
			ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
		}

		ROM_SysCtlDelay(100000);


	}
}


void Timer0IntHandler(void)
{
	// Clear the timer interrupt
	ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

	// Read the current state of the GPIO pin and
	// write back the opposite state
	if(ROM_GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_2))
	{
		ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0);
	}
	else
	{
		ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 4);
	}
}

void ADC0IntHandler(void)
{
	uint32_t ui32ADC0Value[4];
	volatile uint32_t ui32TempAvg;
	volatile uint32_t ui32TempValueC;
	volatile uint32_t ui32TempValueF;
	   ROM_ADCSequenceDataGet(ADC0_BASE, 1, ui32ADC0Value);
	   ui32TempAvg = (ui32ADC0Value[0] + ui32ADC0Value[1] + ui32ADC0Value[2] + ui32ADC0Value[3] + 2)/4;
	   ui32TempValueC = (1475 - ((2475 * ui32TempAvg)) / 4096)/10;
	   ui32TempValueF = ((ui32TempValueC * 9) + 160) / 5;
	ADCIntClear(ADC0_Base,1);


}

  • Hi,

    I am not surprised your ADC is not going to interrupt - you did not enabled the interrupt for ADC. Nor I know it is added to interrupt vectors in your startup_xxx.c file (you should mention that...).

    Other problems - to  have the ADC triggered by timer, there are tow steps in configuration a) the sequencer should use ADC_TRIGGER_TIMER instead your choice and b) the timer shoud be configured to trigger the ADC. I will let you this to discover - read functions in timer.c file. Also, in this case, you do not need to enable the timer interrupt.

    Also if you need an average, there is an oversample mode for ADC.

    Petrei

    Edit: OK, you enabled the ADC interrupt, saw it later...

  • Hello Petrei

    I think you are right. The missing startup file would indicate that the poster never did add it to the file.

    Regards
    Amit