Other Parts Discussed in Thread: TM4C123GH6PM
#define GPIO_PORTF_DATA_R (*((volatile unsigned long *)0x400253FC))
#define GPIO_PORTF_DIR_R (*((volatile unsigned long *)0x40025400))
#define GPIO_PORTF_AFSEL_R (*((volatile unsigned long *)0x40025420))
#define GPIO_PORTF_PUR_R (*((volatile unsigned long *)0x40025510))
#define GPIO_PORTF_DEN_R (*((volatile unsigned long *)0x4002551C))
#define GPIO_PORTF_LOCK_R (*((volatile unsigned long *)0x40025520))
#define GPIO_PORTF_CR_R (*((volatile unsigned long *)0x40025524))
#define GPIO_PORTF_AMSEL_R (*((volatile unsigned long *)0x40025528))
#define GPIO_PORTF_PCTL_R (*((volatile unsigned long *)0x4002552C))
#define SYSCTL_RCGC2_R (*((volatile unsigned long *)0x400FE108))
#define PF0 (*((volatile unsigned long *)0x40025004)) // defining port F bit 0
#define PF1 (*((volatile unsigned long *)0x40025008)) // defining port F bit 1
void PortF_Init(void){ volatile unsigned long delay;
SYSCTL_RCGC2_R |= 0x00000020; // 1) F clock
delay = SYSCTL_RCGC2_R; // delay to activate clock
GPIO_PORTF_LOCK_R = 0x4C4F434B; // 2) unlock PortF PF0
GPIO_PORTF_CR_R = 0x1F; // allow changes to PF4-0
GPIO_PORTF_AMSEL_R = 0x00; // 3) disable analog function
GPIO_PORTF_PCTL_R = 0x00000000; // 4) GPIO clear bit PCTL
GPIO_PORTF_DIR_R = 0x0E; // 5) PF4,PF0 input, PF3,PF2,PF1 output
GPIO_PORTF_AFSEL_R = 0x00; // 6) no alternate function
GPIO_PORTF_PUR_R = 0x11; // enable pullup resistors on PF4,PF0
GPIO_PORTF_DEN_R = 0x1F; // 7) enable digital pins PF4-PF0
}
unsigned long i;
int main(void)
{
PortF_Init();
while(1)
{
if(PF0==0x00) //to check whether switch is pressed or not
{
PF1=0x02; // to send digital 1 to port F bit 1
}
else
PF1=0x00; // to send digital 0 to port F bit 1
}
}