Hello together,
i have issues to set up the ADC and DMA working together, in the way, that the DMA transfers a converted value to a given RAM address.
I´m using ADC0, Sample Sequencer 3; the RAM address is representes by the uint32_t adcVal; variable. The setup for the ADC supposes a software trigger.
Until now i could manage to make up a config, where the ADC runs in software trigger mode, triggers an ISR on "conversionDONE" and starts a DMA software transfer from the SS3 Fifo to the RAM based on the first example in Lab13 of the "TM4C123G_LaunchPad_Workshop_Workbook".
But i´m not able to get this done with the way, that the ADC sends a request to the DMA. I have inserted comments at points where i´m not sure if it is correct what i´m doing.
First it follows just the config routines and at the bottom the complete code.
#define SEQUENCER3 3 #define AMT_OF_ITEMS 1 // Set up clocking System ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ); ROM_SysCtlPeripheralClockGating(true); // Set up PIN E1 and E2 for analog input SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1|GPIO_PIN_2); //*************************************************************************************** //************************** Set up ADC ****************************************** //*************************************************************************************** SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); //enable ADC clock ADCSequenceConfigure(ADC0_BASE, SEQUENCER3, ADC_TRIGGER_PROCESSOR, 0); //use SS3, enable software trigger, high priority /* Here i have issue with the ADC_CTL_IE bit. The "TM4C123GH6PM" datasheet says on page 803; chapter 13.3.2.2 "DMA Operation" (last sentence): "A burst transfer request is asserted when the interrupt bit for the sample sequence is set (IE bit in the ADCSSCTLn register is set)." on page 599; chapter 9.2.8 "Peripheral Interface": "Note: When using μDMA to transfer data to and from a peripheral, the peripheral must disable all interrupts to the NVIC." */ ADCSequenceStepConfigure(ADC0_BASE, SEQUENCER3, 0, ADC_CTL_CH2|ADC_CTL_IE|ADC_CTL_END); //define STEP 0 with SS3, use AIN2, Interrupt enable, define step as last sample ADCSequenceEnable(ADC0_BASE, SEQUENCER3); // enable SS3 ADCSequenceDMAEnable(ADC0_BASE, SEQUENCER3); // enable SS3 for DMA //*************************************************************************************** //************************** Set up DMA ****************************************** //*************************************************************************************** /* I´m not sure, if "UDMA_CHANNEL_ADC0" is the correct argument. When searching in the document "spmu36" ROM User Guide for the "ROM_uDMAChannelAttributeDisable" ebtry, it is written, that the the first argument "uint32_t ui32ChannelNum" must be one of the values - UDMA_CHANNEL_ADC0 - UDMA_CHANNEL_ADC1 - UDMA_CHANNEL_ADC2 - UDMA_CHANNEL_ADC3 - UDMA_SEC_CHANNEL_ADC10 - .... What do the values ADC 0 to 4 relate to? Do they cover the existence of up to 4 ADC hardwares or do they relate to the FIFO´s of the 4 Sample Sequencers? Plus when i take a look at their definition in udma.h File of TIVA-C WARE driver library the UDMA_CHANNEL_ADC0 is 14. What does 14 mean? For example according to the datasheet on page 587, chapter 9.2.1 "Channel Assignments" the channel for the ADC0_SS3 (which i´m using) would be 17 and channel 14 is for ADC0_SS0. */ ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0, UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |(UDMA_ATTR_HIGH_PRIORITY | UDMA_ATTR_REQMASK)); ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC0, UDMA_ATTR_USEBURST| UDMA_ATTR_HIGH_PRIORITY); // arbitation size = 1 since there is one value to transfer // also tried UDMA_SRC_INC_NONE, since i don´t transfer to an array ROM_uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_32| UDMA_DST_INC_32 | UDMA_ARB_1); ROM_uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_MODE_AUTO, (void*)(ADC0_BASE + 0xA8),//address of ADC0´s SS3 FIFO &adcVal,// dest address AMT_OF_ITEMS); //AMT_OF_ITEMS = 1 ROM_uDMAControlBaseSet(pui8ControlTable); ROM_uDMAChannelEnable(UDMA_CHANNEL_ADC0); ROM_uDMAChannelAssign(UDMA_CH17_ADC0_3); /* For the following IE´s i´m not sure weather to activate them or not */ ADCIntEnable(ADC0_BASE, SEQUENCER3); IntEnable(INT_ADC0SS3); IntEnable(INT_UDMA); IntMasterEnable(); ADCProcessorTrigger(ADC0_BASE, SEQUENCER3);
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/udma.h"
#include "driverlib/adc.h"
#define SEQUENCER3 3
#define AMT_OF_ITEMS 1
static uint32_t adcVal;
// Define errors counters
static uint32_t g_ui32DMAErrCount = 0;
// The control table used by the uDMA controller. This table must be aligned to a 1024 byte boundary.
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
// Library error routine
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
// uDMA transfer error handler
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
// Check for uDMA error bit
ui32Status = ROM_uDMAErrorStatusGet();
// If there is a uDMA error, then clear the error and increment the error counter.
if(ui32Status)
{
ROM_uDMAErrorStatusClear();
g_ui32DMAErrCount++;
}
}
// Initialize the uDMA software channel to perform a memory to memory uDMA transfer.
void adcConversionSeq3DoneHandler(void)
{
ADCIntClear(ADC0_BASE, SEQUENCER3);
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_AUTO,
(void*)(ADC0_BASE + 0xA8),
&adcVal,
AMT_OF_ITEMS);
ADCProcessorTrigger(ADC0_BASE, SEQUENCER3);
}
int
main(void)
{
volatile int dummy = 0;
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
ROM_SysCtlPeripheralClockGating(true);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1|GPIO_PIN_2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ADCSequenceConfigure(ADC0_BASE, SEQUENCER3, ADC_TRIGGER_PROCESSOR, 0);
//ADCSequenceStepConfigure(ADC0_BASE, SEQUENCER3, 0, ADC_CTL_CH2|ADC_CTL_IE|ADC_CTL_END);
ADCSequenceStepConfigure(ADC0_BASE, SEQUENCER3, 0, ADC_CTL_CH2|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, SEQUENCER3);
ADCSequenceDMAEnable(ADC0_BASE, SEQUENCER3);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_uDMAEnable();
ROM_IntEnable(INT_UDMAERR);
/**/ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0,
UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |
(UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK));
ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC0,
UDMA_ATTR_USEBURST|
UDMA_ATTR_HIGH_PRIORITY);
ROM_uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_SIZE_32 | UDMA_SRC_INC_32| UDMA_DST_INC_32 |
UDMA_ARB_1);
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_AUTO,
(void*)(ADC0_BASE + 0xA8),
&adcVal,
AMT_OF_ITEMS);
ROM_uDMAControlBaseSet(pui8ControlTable);
ROM_uDMAChannelEnable(UDMA_CHANNEL_ADC0);
ROM_uDMAChannelAssign(UDMA_CH17_ADC0_3);
ADCIntEnable(ADC0_BASE, SEQUENCER3);
IntEnable(INT_ADC0SS3);
//IntEnable(INT_UDMA);
IntMasterEnable();
ADCProcessorTrigger(ADC0_BASE, SEQUENCER3);
while(1)
{
}
}