Other Parts Discussed in Thread: UNIFLASH
Hi
I've tested to rm57 HDK by CCS 6.0.1, but it can't write to flash.
below is an error message in console.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: Flash Programmer: Error erasing Bank 0, Sector 0. Operation Cancelled.
CortexR5: Unable to terminate memory download: NULL buffer pointer at 0x3a9f
CortexR5: GEL: File: C:\Test_Work\EFI_RM57\Debug\EFI_RM57.out: Load failed.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
I was executed "Hercules Safety Mcu Demo" in order to solve this problem.
but "Hercules Safety Mcu Demo" was not executed
below is an error message .
Uniflash With Required Hercules Device Support Package was not found on your computer. Please Update your Hercules Device Support Package using the check for updates in the Uniflash Menu and then try again..
I had uniflash verson3.1. but uniflash3.1 is not supported to rm57.
I was see that same problem in forums.
But i could not have solved this problem.
I want to know this problem solution.