This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 I2C Problem

Other Parts Discussed in Thread: HALCOGEN

Hi everyone, I am new to i2c and TMS570. I have some issues developing communication between my TMS570LS3137ZWT and MPL3115A2 pressure sensor using i2c interface. I first use the oscilloscope to check the signal from TMS570 without connecting to the sensor. Here is my setting in HALCoGen: 1. Enable I2C Driver only 2. Check I2C only in Pinmux 3. Others pls check the image below http://i.imgur.com/FTXpMnUl.jpg  http://i.imgur.com/J47o0L3l.jpg http://i.imgur.com/ILXJ3lOl.jpg http://i.imgur.com/e9aPJkll.jpg And for all the case below the own_add is 0x20 I have eight questions about the i2c question: 1. How can I avoid the own_address in the start condition or it is unavoidable? i2cInit(); i2cSetOwnAdd(i2cREG1,own_add); i2cEnableLoopback(i2cREG1); i2cSetStart(i2cREG1); i2cSendByte(i2cREG1,0xFF); while(1); from the above the codding I expected there is only a start condition followed by a oxFF signal,However, the first byte is always the own_add (you can change it by you can't remove). is it normal or is it unavoidable? Case1 - With Setstart and 0xFF http://i.imgur.com/LwTdTnU.jpg Case2 - SetStart without 0xFF http://i.imgur.com/0DeuztY.jpg 2. Why EnableLoopBack function is necessary? from same set of code the EnableLoopBack function is necessary. Without that signal an unknown is found. It is normal? What is the purpose of it? Case3 - EnableLoopBack with 0xAA http://i.imgur.com/GhB5Elb.jpg Case4 - Without EnableLoopBack http://i.imgur.com/nljdZe4.jpg 3) How can I generate the second start condition I try to ignore the own_address and EnableLoopBack issue, I cannot generate the second start condition. Case5 - First Setstart before 0xFF, Second SetStart after 0xFF http://i.imgur.com/RuaFanR.jpg Case6 - First SetStart Only, no second one http://i.imgur.com/BkHkphb.jpg 4) Why I can only send 2 bytes ? In Case 7 there should be 3 0xFF signal but at last only two are generated. Case7 - Three SendByte Function http://i.imgur.com/xEvUL1W.jpg 5) In the official example from HALCoGen, only 8 characters (8 bytes are sent) Case8 - LES http://i.imgur.com/RFllUHZ.jpg Case9 - LEZ http://i.imgur.com/KAFGBrW.jpg 6) I cannot generate a Stop Condition Case10 - With SetStop function http://i.imgur.com/m15N3bF.jpg Case11 - Without SetStop function http://i.imgur.com/JY02owC.jpg 7) ~transmitter I set ~ transmitter after 0xFF, but the changes appear before 0xFF. How does it happen? Case 12 - with ~I2CTRANSMITTER after 0xFF http://i.imgur.com/6DN7YLu.jpg Case13 - without ~I2CTRANSMITTER after 0xFF http://i.imgur.com/MfMSYDq.jpg 8) Ack Bit In fact the TMS570 only connected to oscilloscope. I expected that the ack bit is always 1 as no sensor is present. However, in all the case above the ack bit is always 0, how does it happen? At last, I just want to generate a basic communication like: Start Condition - Slave Address Write - Start Condition - Slave Address Read - Feedback from Sensor - Stop Can you suggest how can I do this? Thanks for your kind attention. Man Choi