This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugger hangs on loading TM4C1294XL Launchpad

I am currently evaluating the TM4C1294 process for use in an upcoming project using the Launchpad for it.  I am debugging using the included in circuit debugger on the launchpad board.  When working with any of the example projects or projects that I have created, the debugger hangs for over 30 seconds on the Launching Debug Session step.  The progress bar is full and says "Launching 100%" but the system hangs at that point.  After 30 seconds or so the debugger continues loading as expected and runs fine from there.

I have tried debug the same project and code from IAR and the debugger loads in a few seconds so there is no issue with the board or debugger as far as I can tell.

Is there anything that can be done to speed up the debugger or is this a known issue with these boards?

If it helps I am running this on CCSv5.5.0 on Windows 8.1.

Thanks,

Patrick

  • Hello Patrick,

    What is the size of the image being loaded? The speed cannot be changed for the ICDI on the launchpad.

    Regards
    Amit
  • Suggest that you look at two areas:

    a)  Might you have changed any of the factory - IDE settings - tying your MCU to the IDE?   Even a subtle "miscue" may trigger such delay.

    It's very important that you, "Test & try to repeat this behavior with a "pure, factory supplied project - ideally one of the smaller, simpler ones."

    b) Have you a separate MCU board?  Should the issue persist across two such boards - I'd bet on some IDE mis-setting.  If the issue clears w/a fresh board - look for a board gremlin.

  • This happens with any project that I try to load to the board including the bitband example that is < 30K or so.
  • Hello Patrick,

    I think then the IDE is the problem (as cb1 also mentioned). Might I suggest uninstalling CCSv5, deleting all of its contents in history, cache, temp, etc... and checking it with a CCSv6 or fresh copy of CCSv5.5 on your machine. Also did you check the same with a Win-7 machine?

    Regards
    Amit