Other Parts Discussed in Thread: TM4C123GH6PM
Hi All,
I am using TM4C123GH6PM part in one of the project,
The requirement is to implement shutdown feature for the system. The shutdown could be in the following sequence (suggest me if there is any better sequence):
- Disable all peripherals ICs
- Disable the microcontroller system clock
- Enter into sleep mode
I would like to know hardware setup also as I am not sure what would be the behavior of the nWAKE pin when controller is active state. I am using a single reset like switch. Can I connect it to nWAKE pin to put the system in shutdown on press and wake the controller and boot it once again on next press?
Is there any interrupt handler for nWAKE pin during active state of the controller.
Please help me as this concept is new to me.
For any more info feel free to ask me.
Looking forward to hear from you soon.
Regards
Anand M