This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNLOCK problem with TM4C123GH6M PF0 Pin



Im using PF0 pin as SSI1 RX function, but PF0 default is NMI. I write the unlock PF0 code as the example showed in forum as follows. HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY; //Unlock HWREG(GPIO_PORTF_BASE+GPIO_O_CR) |= 0X01; // Enable PF0 AFS SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1); GPIOPinConfigure(GPIO_PF0_SSI1RX); HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) =0; // Relock It works well on the first time the program is debugged and PF0 is working as SSI1RX. But when the target board is reset or re-power on. The TM4C123G does not work and runs into a fault ISR which led to an infinite loop. After this it never works again, unless we comment the unlock program code. But if we do this, the PF0 function is default to NMI pin again. How can I permanently set PF0 to SSI1RX function?
  • Hello user4085323,

    The code was smashed on your post, so a little bit of copy-paste-edit. Can you please confirm this is your code.

    HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY; //Unlock
    HWREG(GPIO_PORTF_BASE+GPIO_O_CR) |= 0X01; // Enable PF0 AFS
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
    GPIOPinConfigure(GPIO_PF0_SSI1RX);
    HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) =0; // Relock

    The issue is that the peripheral enable is being done after enabling Port-F. The correct code would be

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
    HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY; //Unlock
    HWREG(GPIO_PORTF_BASE+GPIO_O_CR) |= 0X01; // Enable PF0 AFS
    HWREG(GPIO_PORTF_BASE+GPIO_O_LOCK) =0; // Relock
    GPIOPinConfigure(GPIO_PF0_SSI1RX);

    Regards
    Amit