This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hibernation clock in TM4C123GH6PM

Hi, 

In the below code i have used System clock for Hibernation module,

so i want to know whether the device will be using the same frequency after it goes into hibernation ???

#include <stdint.h>
#include <stdbool.h>
#include "utils/ustdlib.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/debug.h"
#include "driverlib/hibernate.h"
#include "driverlib/gpio.h"

int main(void)
{
	SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);

	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
	GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
	GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x08);

	SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);
	HibernateEnableExpClk(SysCtlClockGet());
	HibernateGPIORetentionEnable();
	SysCtlDelay(64000000);
	HibernateWakeSet(HIBERNATE_WAKE_PIN);
	GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0x00);

	HibernateRequest();
	while(1)
	{
	}
}