This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing of Stepper motor with TM4C123GH6PM

I am using  Tiva C series TM4C123G LaunchPad Evaluation Kit to control direction of stepper motor depending upon UART signal. Input "12" for clockwise direction and input "13" for anticlockwise.

1) In windows,

When I directly write to the port using command prompt .  echo 12> com3 and echo 13>com3   , stepper motor rotates perfectly.

2)In Linux,

Kit is detected as "/dev/ttyACM0" . When I am directly trying to write to device using  " echo 12> /dev/ttyACM0" .Motordoes not spin.

Any suggestions why motor is not running in LInux? Is I am missing something?

Thanks,

Tushar