Hi, I have been trying to get the following example code to work
//***************************************************************************** // // uart_echo.c - Example for reading data from and writing data to the UART in // an interrupt driven fashion. // // Copyright (c) 2013-2014 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // // This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package. // //***************************************************************************** #include <stdint.h> #include <stdbool.h> #include "inc/hw_ints.h" #include "inc/hw_memmap.h" #include "driverlib/debug.h" #include "driverlib/gpio.h" #include "driverlib/interrupt.h" #include "driverlib/pin_map.h" #include "driverlib/rom.h" #include "driverlib/rom_map.h" #include "driverlib/sysctl.h" #include "driverlib/uart.h" //***************************************************************************** // //! \addtogroup example_list //! <h1>UART Echo (uart_echo)</h1> //! //! This example application utilizes the UART to echo text. The first UART //! (connected to the USB debug virtual serial port on the evaluation board) //! will be configured in 115,200 baud, 8-n-1 mode. All characters received on //! the UART are transmitted back to the UART. // //***************************************************************************** //**************************************************************************** // // System clock rate in Hz. // //**************************************************************************** uint32_t g_ui32SysClock; //***************************************************************************** // // The error routine that is called if the driver library encounters an error. // //***************************************************************************** #ifdef DEBUG void __error__(char *pcFilename, uint32_t ui32Line) { } #endif //***************************************************************************** // // The UART interrupt handler. // //***************************************************************************** void UARTIntHandler(void) { uint32_t ui32Status; // // Get the interrrupt status. // ui32Status = ROM_UARTIntStatus(UART0_BASE, true); // // Clear the asserted interrupts. // ROM_UARTIntClear(UART0_BASE, ui32Status); // // Loop while there are characters in the receive FIFO. // while(ROM_UARTCharsAvail(UART0_BASE)) { // // Read the next character from the UART and write it back to the UART. // ROM_UARTCharPutNonBlocking(UART0_BASE, ROM_UARTCharGetNonBlocking(UART0_BASE)); // // Blink the LED to show a character transfer is occuring. // GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0); // // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks. // SysCtlDelay(g_ui32SysClock / (1000 * 3)); // // Turn off the LED // GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0); } } //***************************************************************************** // // Send a string to the UART. // //***************************************************************************** void UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count) { // // Loop while there are more characters to send. // while(ui32Count--) { // // Write the next character to the UART. // ROM_UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++); } } //***************************************************************************** // // This example demonstrates how to send a string of data to the UART. // //***************************************************************************** int main(void) { // // Set the clocking to run directly from the crystal at 120MHz. // g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000); // // Enable the GPIO port that is used for the on-board LED. // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION); // // Enable the GPIO pins for the LED (PN0). // ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0); // // Enable the peripherals used by this example. // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Enable processor interrupts. // ROM_IntMasterEnable(); // // Set GPIO A0 and A1 as UART pins. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Configure the UART for 115,200, 8-N-1 operation. // ROM_UARTConfigSetExpClk(UART0_BASE, g_ui32SysClock, 115200, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); // // Enable the UART interrupt. // ROM_IntEnable(INT_UART0); ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT); // // Prompt for text to be entered. // UARTSend((uint8_t *)"\033[2JEnter text: ", 16); // // Loop forever echoing data through the UART. // while(1) { } }
Some things to know:
I am using the TM4C1294XL launchpad and i have it hooked up to my computer via the debug usb. The terminal i am using is realterm. I have set the baudrate to 115200 with 8 bits 1 stop bit and no partiy. The comport is the right one being used (inn my came Com9). I am using windows 7.
Here is the problem:
Every time i enter a key stroke the realterm diplays F8 FB (The F8 chages with different key strokes, I think that is supposed to be illegal character.
I ran through the code putting break points at UARTIntHandler(), UARTSend(), and inside of main right at the UARTSend() call.
Putting aside the whole input output that supposed to occur, i only tried to focus on the UartSend() call to see what was going on code wise.
As i stepped though the call i see that the function takes two arguments: the first is supposed to be the strings first characters Address via a pointer, and the second is the string length so the while loop can out put the string one character at a time (this is my understanding).
The statement inside the while loop, ROM_UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++), i am assuming that it uses *puiBudder++ to go through the string buffer and i am guessing that the UART0_BASE is the FIFO queue for the UART.
I am guessing that the function is taking the string character and placing it into the queue one letter at a time.
I hope i understood this correctly. So now my problem is:
Why does the UARSend() call have (uint8_t *)"/033[2JEnter Text: " as the first argument?
Also What is the code doing to the characters in the queue, i see that the UARTIntHandler is rewriting stuff back to the Queue. Does the Terminal read from that queue on its own?
Here is what the out put is for the UARTSend() in hex: 3B ED FA 73 0A
Here is the outputs for the key strokes:
q: F9 FF
w: FF FF
e: FD FB
r: FA FF
t: FC FF
y: F9 FF (it repeats)
u: FD FF
i: F9 FB
o: FF FB
p: F8 FF
a: F9 FB
s: FB FF
d: FC FB
f: FE FB
g: FF FB
h: F8 FB
j: FA FB
k: FB FB
l: FC FB
z: FA FF
x: F8 FF
c: FB FB
v: FE FF
b: FA FB
n: FE FB
m: FD FB
0: F8 FE
1: F9 FE
2: FA FE
3: FB FE
4: FC FE
5: FD FE
6: FE FE
7: FF FE
8: F8 FE
9: F9 FE