Other Parts Discussed in Thread: TM4C123GH6PM
Hi,
I have tried several times altering the I2C code in many possible ways
but i am still not able to get it to communicate with another tiva board TM4C123GH6PM (slave).
Then i tried receiving the SDA and SCL with an oscilloscope, but the SDA line copies the SCL.
Any idea why this is happening ?
The master code is embedded below.
Thanks in advance.
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
// Number of I2C data packets to send.
#define NUM_I2C_DATA 3
#define SLAVE_ADDRESS 0x3C
void InitConsole(void)
{
//
// Enable GPIO port A which is used for UART0 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Configure the pin muxing for UART0 functions on port A0 and A1.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//
// Enable UART0 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
int main()
{
uint32_t pui32DataRx[NUM_I2C_DATA];
uint32_t reverse[NUM_I2C_DATA];
uint32_t ui32Index, i;
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
//I2CSlaveInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
//I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
I2CSlaveEnable(I2C0_BASE);
I2CSlaveInit(I2C0_BASE, SLAVE_ADDRESS);
InitConsole();
while(1)
{
UARTprintf("1\n");
//while(!(I2CSlaveStatus(I2C0_BASE) & I2C_SLAVE_ACT_RREQ))
// ;
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
UARTprintf("3\n");
while(!(I2CSlaveStatus(I2C0_BASE)))
{
SysCtlDelay(1000000);
UARTprintf(".");
}
pui32DataRx[ui32Index] = I2CSlaveDataGet(I2C0_BASE);
UARTprintf("Received: '%c'\n", pui32DataRx[ui32Index]);
}
// reverse
for(i = 0; i < NUM_I2C_DATA; i++)
reverse[i] = pui32DataRx[NUM_I2C_DATA - i];
UARTprintf("Reversed String: %s\n ", reverse);
UARTprintf("5\n");
// dummy receive
//I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//UARTprintf("2\n");
while(!(I2CSlaveStatus(I2C0_BASE) & I2C_SLAVE_ACT_TREQ))
;
UARTprintf("6\n");
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
UARTprintf("4\n");
UARTprintf(" Sending: '%c' . . . ", reverse[ui32Index]);
I2CSlaveDataPut(I2C0_BASE, reverse[ui32Index]);
while(!(I2CSlaveStatus(I2C0_BASE)))
;
}
}
}