Hi,
We are in the process of development of Safety Class SIL4 certified systems for which I am planning to use Hercules ARM Cortex R4/R5.
We are concerned about the followings:-
1) Whether RTOS is mandatory to be used for such controllers full utilization in a smooth way or whether without RTOS enough support is available. I mean how do people normally go about it. We want to avoid RTOS to avoid the complexity of CENELEC verification of RTOS and the cost associated with it. We do not plan to use TCP-IP stack and USB stack for our system rather simple serial RS422/485 for communication or converted to optical output.
If RTOS is at all necessary then which RTOS is best suggested in terms of price and essential documents such as SIL3/SIL4 certification.
2) Whether the controllers will remain there - i.e. whether silicon and support will be available for coming 5 years or so for these as we have burnt our hands badly with stellaris series.
3) Is there some low cost way for CENELEC SIL3-SIL4 verification of the application software to be developed for the systems from TI or one has to get it verified and validated using tools such as parasoft c/c++ or vector cast or LDRA etc.
Kindly guide us in this. We will be thankful.
Many Regards.
MOHIT.