This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD TFT Touchscreen - Controlling brightness

Other Parts Discussed in Thread: TM4C129XNCZAD

I am working with the TM4C129XNCZAD evaluation board and I need to be able to increase the brightness of the screen. Is this possible and if so, how do you do it? 

  • Hello Marshall,

    Please see the DK-TM4C129 User Guide for LCD Section. The jumper which by default is in 1-2 position needs to be put into 2-3 position. Then a PWM wave of 50K-100K can be applied via the TM4C129 PWM Controller. The DC of the PWM pulse will cause the brightness to be adjusted.

    Regards
    Amit