I have a custom board with a TM4C1294KCPDT. I'm using a XDS200 Emulator.
When I program and debug using the XDS200 the board works as expected.
When I quit the debugger the board keeps running. When I then power the board down and back up, the board does not start. This happens with the Emulator connected or disconnected.
I have configured BOOTCFG to use a push button to enter the USB boot loader. When I power up the board while holding the button the device will show up in the LM Flash Programmer's device list. (LM Flash Build 1613)
However, when I select a BIN file and click the Program button it will show Programming... 0% and give a USB Error: "An error occurred during USB download!".
I have implemented a USB MSC device and it is working correctly so I'm sure the USB interface is working correctly.
Any suggestions on how I debug this issue?
Thanks in advance for your help,
Paul.