This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there is any Military or space grade equivalent available for TM4C123GXL...??



i've been working on my Final year project which is to build a Power Conditioning unit of a Low earth orbit satellite. as an embedded platform we've to use some micro-controller which should be either military grade or space grade so that it can pass pre-launch tests and can be launched in space. i've chosen TM4C123GXL, but i came to know that it is not a military grade so now i want to know that is there any military grade or space grade equivalent available (equivalent to TM4C123GXL), if not then what military grade or space grade micro controllers do TI have with M4 processors