This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't view the variable value whose address is in EPI SDRAM in CCS debugger



Hi

I am debugging my external EPI SDRAM. I am using 1294. I met one problem: I can't view the variable value whose address is within the EPI adress space.

Any way to get out? Thanks

  • Hello Jianyi,

    You need to change the gel file to be able to do so.

    In the debugger go to Tools -> Gel Files

    Double clock the tm4c???.gel file and in the macro memorymap_init() add the following lines at the end of the memory map

    GEL_MapAddStr(0x60000000, 0, 0x01000000, "R|W", 0); /* SDRAM */


    Regards
    Amit
  • Thanks. It works now.

  • Hi, Amit,

      My SDRAM has a strange problem:

      Using memory browser, I can see that the value of address :

    1. 0x60000000, 0x60000200, 0x60000400 and 0x60000600 are the same, but not the same with 0x60000800.
    2. 0x60000002, 0x60000202, 0x60000402 and 0x60000602 are the same, but not the same with 0x60000802.
    3. 0x60000800, 0x60000A00, 0x60000C00 and 0x60000E00 are the same, but not the same with 0x60001000.

    That is, if I change the value of 0x60000000 to some value, 0xFFFF for example, the value of at address 0x60000200/0x60000400/0x60000600 will also be 0xFFFF, but the value of 0x60000800 remains unchanged. Please see the figure below.


         So it looks like A9 and A10 is not working. But I can see that the signal level of A9 and A10 is changing using oscilloscope, and the waveform seems not much different with other address lines. And I also checked that they are not shorted together using a multi-meter.

        My source code is a modified version of "C:\ti\TivaWare_C_Series-2.1.0.12573\examples\peripherals\epi\sdram.c". The main difference is that I use PP2/PP3 for EPI0S29/30, while the example use PN2/PN3. The following is my code:

    //*****************************************************************************
    //
    // sdram.c - Example demonstrating how to configure the EPI bus in SDRAM
    //           mode.
    //
    // Copyright (c) 2014 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    // 
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the  
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.1.0.12573 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_epi.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "inc/hw_gpio.h"
    #include "driverlib/epi.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    
    typedef uint16_t uint16;
    typedef uint32_t uint32;
    
    
    //*****************************************************************************
    //
    //! \addtogroup epi_examples_list
    //! <h1>EPI SDRAM Mode (sdram)</h1>
    //!
    //! This example shows how to configure the TM4C129 EPI bus in SDRAM mode.  It
    //! assumes that a 64Mbit SDRAM is attached to EPI0.
    //!
    //! For the EPI SDRAM mode, the pinout is as follows:
    //!     Address11:0 - EPI0S11:0
    //!     Bank1:0     - EPI0S14:13
    //!     Data15:0    - EPI0S15:0
    //!     DQML        - EPI0S16
    //!     DQMH        - EPI0S17
    //!     /CAS        - EPI0S18
    //!     /RAS        - EPI0S19
    //!     /WE         - EPI0S28
    //!     /CS         - EPI0S29
    //!     SDCKE       - EPI0S30
    //!     SDCLK       - EPI0S31
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - EPI0 peripheral
    //! - GPIO Port A peripheral (for EPI0 pins)
    //! - GPIO Port B peripheral (for EPI0 pins)
    //! - GPIO Port C peripheral (for EPI0 pins)
    //! - GPIO Port G peripheral (for EPI0 pins)
    //! - GPIO Port K peripheral (for EPI0 pins)
    //! - GPIO Port L peripheral (for EPI0 pins)
    //! - GPIO Port M peripheral (for EPI0 pins)
    //! - GPIO Port P peripheral (for EPI0 pins)
    //! - EPI0S0  - PK0
    //! - EPI0S1  - PK1
    //! - EPI0S2  - PK2
    //! - EPI0S3  - PK3
    //! - EPI0S4  - PC7
    //! - EPI0S5  - PC6
    //! - EPI0S6  - PC5
    //! - EPI0S7  - PC4
    //! - EPI0S8  - PA6
    //! - EPI0S9  - PA7
    //! - EPI0S10 - PG1
    //! - EPI0S11 - PG0
    //! - EPI0S12 - PM3
    //! - EPI0S13 - PM2
    //! - EPI0S14 - PM1
    //! - EPI0S15 - PM0
    //! - EPI0S16 - PL0
    //! - EPI0S17 - PL1
    //! - EPI0S18 - PL2
    //! - EPI0S19 - PL3
    //! - EPI0S28 - PB3
    //! - EPI0S29 - PP2
    //! - EPI0S30 - PP3
    //! - EPI0S31 - PK5
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of EPI0.
    //! - UART0 peripheral
    //! - GPIO Port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - None.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Use the following to specify the GPIO pins used by the SDRAM EPI bus.
    //
    //*****************************************************************************
    #define EPI_PORTA_PINS (GPIO_PIN_7 | GPIO_PIN_6)
    #define EPI_PORTB_PINS (GPIO_PIN_3)
    #define EPI_PORTC_PINS (GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_5 | GPIO_PIN_4)
    #define EPI_PORTG_PINS (GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTK_PINS (GPIO_PIN_5 | GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 |   \
                            GPIO_PIN_0)
    #define EPI_PORTL_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTM_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTP_PINS (GPIO_PIN_3 | GPIO_PIN_2)
    
    //*****************************************************************************
    //
    // The starting and ending address for the 64MB SDRAM chip (32Meg x 16bits) on
    // the SDRAM daughter board.
    //
    //*****************************************************************************
    #define SDRAM_START_ADDRESS 0x00000000
    #define SDRAM_END_ADDRESS   0x01FFFFFF
    
    //*****************************************************************************
    //
    // The Mapping address space for the EPI SDRAM.
    //
    //*****************************************************************************
    #define SDRAM_MAPPING_ADDRESS 0x60000000
    
    //*****************************************************************************
    //
    // A pointer to the EPI memory aperture.  Note that g_pui16EPISdram is declared
    // as volatile so the compiler should not optimize reads out of the image.
    //
    //*****************************************************************************
    static volatile uint16_t *g_pui16EPISdram;
    
    //*****************************************************************************
    //
    // A table used to determine the EPI clock frequency band in use.
    //
    //*****************************************************************************
    typedef struct
    {
        uint32_t ui32SysClock;
        uint32_t ui32FreqFlag;
    }
    tSDRAMFreqMapping;
    
    static tSDRAMFreqMapping g_psSDRAMFreq[] =
    {
        //
        // SysClock >= 100MHz, EPI clock >= 50Mhz (divided by 2)
        //
        {100000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 60MHz, EPI clock >= 30MHz (divided by 2)
        //
        {60000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 50MHz, EPI clock >= 50MHz (no divider)
        //
        {50000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 30MHz, EPI clock >= 30MHz (no divider)
        //
        {30000000, EPI_SDRAM_CORE_FREQ_30_50},
    
        //
        // SysClock >= 15MHz, EPI clock >= 15MHz (no divider)
        //
        {15000000, EPI_SDRAM_CORE_FREQ_15_30},
    
        //
        // SysClock < 15Mhz, EPI clock < 15Mhz (no divider)
        //
        {0, EPI_SDRAM_CORE_FREQ_0_15}
     };
    
    #define NUM_SDRAM_FREQ (sizeof(g_psSDRAMFreq) / sizeof(tSDRAMFreqMapping))
    
    
    //*****************************************************************************
    //
    // Configure EPI0 in SDRAM mode.  The EPI memory space is setup using an a
    // simple C array.  This example shows how to read and write to an SDRAM card
    // using the EPI bus in SDRAM mode.
    //
    //*****************************************************************************
    void Board_initSdram(void)
    {
        uint32_t ui32Val, ui32Freq, ui32SysClock;
    
        //
        // Set the clocking to run at 120MHz from the PLL.
        // TODO: Update this call to set the system clock frequency your
        // application requires.
        //
    #if 0
        Types_FreqHz sysFreq;
        Timestamp_getFreq(&sysFreq);
    
        ui32SysClock = sysFreq.lo;
    #else
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_OSC_INT | SYSCTL_USE_PLL |
                                          SYSCTL_CFG_VCO_320), 60000000);
    #endif
    
        //
        // The EPI0 peripheral must be enabled for use.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);
    
        //
        // For this example EPI0 is used with multiple pins on PortA, B, C, G, H,
        // K, L, M and P.  The actual port and pins used may be different on your
        // part, consult the data sheet for more information.
        // TODO: Update based upon the EPI pin assignment on your target part.
        //
    
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
    
        //
        // This step configures the internal pin muxes to set the EPI pins for use
        // with EPI.  Please refer to the datasheet for more information about pin
        // muxing.  Note that EPI0S27:20 are not used for the EPI SDRAM
        // implementation.
        // TODO: Update this section based upon the EPI pin assignment on your
        // target part.
        //
    
        //
        // EPI0S4 ~ EPI0S7: C4 ~ 7
        //
        ui32Val = HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL);
        ui32Val &= 0x0000FFFF;
        ui32Val |= 0xFFFF0000;
        HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S8 ~ EPI0S9: A6 ~ 7
        //
        ui32Val = HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL);
        ui32Val &= 0x00FFFFFF;
        ui32Val |= 0xFF000000;
        HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S10 ~ EPI0S11: G0 ~ 1
        //
        ui32Val = HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFFFF00;
        ui32Val |= 0x000000FF;
        HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S12 ~ EPI0S15: M0 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0000;
        ui32Val |= 0x0000FFFF;
        HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S16 ~ EPI0S19: L0 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0000;
        ui32Val |= 0x0000FFFF;
        HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S28 : B3
        //
        ui32Val = HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0FFF;
        ui32Val |= 0x0000F000;
        HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S29 ~ EPI0S30: P2 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTP_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF00FF;
        ui32Val |= 0x0000FF00;
        HWREG(GPIO_PORTP_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S00 ~ EPI0S03, EPI0S31 : K0 ~ 3, K5
        //
        ui32Val = HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFF0F0000;
        ui32Val |= 0x00F0FFFF;
        HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // Configure the GPIO pins for EPI mode.  All the EPI pins require 8mA
        // drive strength in push-pull operation.  This step also gives control of
        // pins to the EPI module.
        //
        GPIOPinTypeEPI(GPIO_PORTA_BASE, EPI_PORTA_PINS);
        GPIOPinTypeEPI(GPIO_PORTB_BASE, EPI_PORTB_PINS);
        GPIOPinTypeEPI(GPIO_PORTC_BASE, EPI_PORTC_PINS);
        GPIOPinTypeEPI(GPIO_PORTG_BASE, EPI_PORTG_PINS);
        GPIOPinTypeEPI(GPIO_PORTK_BASE, EPI_PORTK_PINS);
        GPIOPinTypeEPI(GPIO_PORTL_BASE, EPI_PORTL_PINS);
        GPIOPinTypeEPI(GPIO_PORTM_BASE, EPI_PORTM_PINS);
        GPIOPinTypeEPI(GPIO_PORTP_BASE, EPI_PORTP_PINS);
    
        //
        // Is our current system clock faster than we can drive the SDRAM clock?
        //
        if(ui32SysClock > 60000000)
        {
            //
            // Yes. Set the EPI clock to half the system clock.
            //
            EPIDividerSet(EPI0_BASE, 1);
        }
        else
        {
            //
            // With a system clock of 60MHz or lower, we can drive the SDRAM at
            // the same rate so set the divider to 0.
            //
            EPIDividerSet(EPI0_BASE, 0);
        }
    
        //
        // Sets the usage mode of the EPI module.  For this example we will use
        // the SDRAM mode to talk to the external 64MB SDRAM daughter card.
        //
        EPIModeSet(EPI0_BASE, EPI_MODE_SDRAM);
    
        //
        // Keep the compiler happy by setting a default value for the frequency
        // flag.
        //
        ui32Freq = g_psSDRAMFreq[NUM_SDRAM_FREQ - 1].ui32FreqFlag;
    
        //
        // Examine the system clock frequency to determine how to set the SDRAM
        // controller's frequency flag.
        //
        for(ui32Val = 0; ui32Val < NUM_SDRAM_FREQ; ui32Val++)
        {
            //
            // Is the system clock frequency above the break point in the table?
            //
            if(ui32SysClock >= g_psSDRAMFreq[ui32Val].ui32SysClock)
            {
                //
                // Yes - remember the frequency flag to use and exit the loop.
                //
                ui32Freq = g_psSDRAMFreq[ui32Val].ui32FreqFlag;
                break;
            }
        }
    
        //
        // Configure the SDRAM mode.  We configure the SDRAM according to our core
        // clock frequency.  We will use the normal (or full power) operating
        // state which means we will not use the low power self-refresh state.
        // Set the SDRAM size to 64MB with a refresh interval of 1024 clock ticks.
        //
        EPIConfigSDRAMSet(EPI0_BASE, (ui32Freq | EPI_SDRAM_FULL_POWER |
                          EPI_SDRAM_SIZE_512MBIT), 200);
    
        //
        // Set the address map.  The EPI0 is mapped from 0x60000000 to 0x01FFFFFF.
        // For this example, we will start from a base address of 0x60000000 with
        // a size of 256MB.  Although our SDRAM is only 64MB, there is no 64MB
        // aperture option so we pick the next larger size.
        //
        EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_256MB | EPI_ADDR_RAM_BASE_6);
    
        //
        // Wait for the SDRAM wake-up to complete by polling the SDRAM
        // initialization sequence bit.  This bit is true when the SDRAM interface
        // is going through the initialization and false when the SDRAM interface
        // it is not in a wake-up period.
        //
        while(HWREG(EPI0_BASE + EPI_O_STAT) &  EPI_STAT_INITSEQ)
        {
        }
    
        //
        // Set the EPI memory pointer to the base of EPI memory space.  Note that
        // g_pui16EPISdram is declared as volatile so the compiler should not
        // optimize reads out of the memory.  With this pointer, the memory space
        // is accessed like a simple array.
        //
        g_pui16EPISdram = (uint16_t *)0x60000000;
    
        g_pui16EPISdram[0] = 0x1234;
        g_pui16EPISdram[1] = 0x5678;
        g_pui16EPISdram[2] = 0x1010;
    
        uint16 read_val = g_pui16EPISdram[0];
        read_val = g_pui16EPISdram[1];
        read_val = g_pui16EPISdram[2];
    
        //
        // Read the initial data in SDRAM, and display it on the console.
        //
    
        //test sdram
        uint16 testVal_Saved = 0;
    
        while(1)
        {
          uint32 testSize = 0x300;
    
          uint32 addressOffset = 0x0000;
    
          uint32 startAddr = SDRAM_MAPPING_ADDRESS + addressOffset;
    
          uint16 testVal = testVal_Saved;
    
          for(g_pui16EPISdram = (uint16_t *)startAddr; 
              g_pui16EPISdram < (uint16_t *)(startAddr + testSize);
              g_pui16EPISdram++)
          {
            *g_pui16EPISdram = testVal++;
          }
    
          testVal = testVal_Saved;
          for(g_pui16EPISdram = (uint16_t *)startAddr; 
              g_pui16EPISdram < (uint16_t *)(startAddr + testSize);
              g_pui16EPISdram++)
          {
            const uint16 testVal_Read = *g_pui16EPISdram;
            if(testVal_Read != testVal++)
            {
              break;
            }
          }
    
          testVal_Saved = testVal;
        }
      
        return;
    }
    

    Can you help check what is the problem? I am using W9864G6KH, and the datasheet is attached.

    Thank you very much.

    W9864G6KH.pdf

     

  • Hello Jianyi,

    If you don't use the memory browser but rely on the program to write the values then does the WR/RD check Pass?

    Regards
    Amit
  • No. The failure is exactly the same.
  • Hello Jianyi,

    Can you share the schematics of the design especially the interfacing of the TM4C129 and the SDRAM memory.

    Regards
    Amit
  • Can you give me your email so that I could send it to you?
  • Hello Jianyi,

    I have sent a Conversation Request. You can attach the schematics to the same. I will review and send my inputs to see what is not working. Possibly, I may request some experiment and waveforms as well if you have a LA handy.

    Regards
    Amit
  • Hello Jianyi,

    Based on the schematic, data sheet and review of the software configuration, the issue appears to be the fact that a 64Mbit memory is connected but the configuration is for a 512Mb memory. The change to the configuration must be

    //
    // Configure the SDRAM mode. We configure the SDRAM according to our core
    // clock frequency. We will use the normal (or full power) operating
    // state which means we will not use the low power self-refresh state.
    // Set the SDRAM size to 16MB with a refresh interval of 1024 clock ticks.
    //
    EPIConfigSDRAMSet(EPI0_BASE, (ui32Freq | EPI_SDRAM_FULL_POWER |
    EPI_SDRAM_SIZE_64MBIT), 850);
    //
    // Set the address map. The EPI0 is mapped from 0x60000000 to 0x01FFFFFF.
    // For this example, we will start from a base address of 0x60000000 with
    // a size of 256MB. Although our SDRAM is only 64MB, there is no 64MB
    // aperture option so we pick the next larger size.
    //
    EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_16MB | EPI_ADDR_RAM_BASE_6);

    Regards
    Amit
  • Thank you very much. Now it works perfectly.
  • Hello Jianyi,

    Thanks for the confirmation.

    Regards
    Amit