Hello,
as part of our evaluation of the TMS570LC43x family we are testing the MibSPI DMA functionality using the TMDX570LC43HDK. We are using the example included with HALCoGen (example_mibspiDMA.c) but the DMA transfer does not succeed (RXDATA remains zero). We have created the project with HALCoGen as described in the example, and are using the completely unmodified file "example_mibspiDMA.c".
Is there a known issues with MibSPI DMA transfers on this chip, or the code created by HALCoGen, or the example?
The toolchain we are using is as follows:
HALCoGen: 04.02.00
Code Composer Studio: 6.0.1.00040
Compiler: TI v5.2.0
Any help would be greatly appreciated. I am attaching the Code Composer Studio project for reference.