Hi,
I am using Halcogen 4.2 with the TMS570LS0332. When I try to open my project I get a series of errors, but it seems to import correctly. Any idea what is going on or how I can fix it?
Thanks,
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using Halcogen 4.2 with the TMS570LS0332. When I try to open my project I get a series of errors, but it seems to import correctly. Any idea what is going on or how I can fix it?
Thanks,
David
It was probably created on version 4.0. The files are attached, there are no backup files in the directory.
Thanks,
David
I've tried to import this project and generate code from it.
I didn't get errors in the output window.
I did get the same errors (IMy output window didn't show them the first time when I was running it in 'auto-hide' mode)
I'm using 04.02.00
Hi David,
I could not reproduce your Issue..
I created a TMS570LS0332PZ Project with 4.01.00, Opened in 4.02.00 -- It Works Fine with no Error Message
I created a TMS570LS0332PZ Project with 4.00.00, Opened in 4.02.00 -- It Works Fine with no Error Message
The observations of Jan Cumps is the only thing I could think for your issue. Have you by mistake edited or ran over some scripts on the DIL file. If not then try pls to replicate the issue with fresh project, if you still get the issue do let us know.