Other Parts Discussed in Thread: TMS570LC4357, DP83640, HALCOGEN
hi ti,
i am working with tms570lc4357 Ethernet module.
i have to receive a frame from pc and transmit a frame hdk to pc.
1. i have tried for transmission. i did the modifications in the demo code itself. but it goes to data entry. should i enable something??
2. when lwIPInit() is called the sequence that is mentioned in wiki is completed.
it is mentioned in wiki that "Write the RX Header Descriptor Pointer using EMACRxHdrDescPtrWrite(). The EMAC hardware will start receiving data at this point."
so where can i check this??
i am attaching the code with this
/** @file sys_main.c
* @brief Application main file
* @date 15.July.2009
* @version 1.01.000
*
* This file contains the initialization & control path for the LwIP & EMAC driver
* and can be called from system main.
*/
/* (c) Texas Instruments 2011, All rights reserved. */
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
#include "HL_sys_common.h"
#include "HL_system.h"
#include "HL_emac.h"
#include "HL_mdio.h"
#include "HL_phy_dp83640.h"
#include "HL_sci.h"
#include "hdkif.h"
#else
#include "sys_common.h"
#include "system.h"
#include "emac.h"
#include "mdio.h"
#include "phy_dp83640.h"
#include "sci.h"
#endif
#include "lwipopts.h"
#include "lwiplib.h"
#include "httpd.h"
#include "lwip\inet.h"
#include "locator.h"
#define TMS570_MDIO_BASE_ADDR 0xFCF78900u /* Same base address for TMS570 & RM48 devices */
#define TMS570_EMAC_BASE_ADDR 0xFCF78000u /* Same base address for TMS570 & RM48 devices */
#define DPS83640_PHYID 0x20005CE1u /** PHY ID Register 1 & 2 values for DPS83640 (Same for TMS570 & RM devices */
#define PHY_ADDR 1 /** EVM/Hardware dependent & is same for TMS570 & RM48 HDKs */
/* Choosing the SCI module used depending upon the device HDK */
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
#define sciREGx sciREG1
#else
#define sciREGx scilinREG
#endif
uint8_t txtCRLF[] = {'\r', '\n'};
uint8_t txtTitle[] = {"HERCULES MICROCONTROLLERS"};
uint8_t txtTI[] = {"Texas Instruments"};
uint8_t txtLittleEndian[] = {"Little Endian device"};
uint8_t txtBigEndian[] = {"Big Endian device"};
uint8_t txtEnetInit[] = {"Initializing ethernet (DHCP)"};
uint8_t txtIPAddrTxt[] = {"Device IP Address: "};
uint8_t txtNote1[] = {"Webserver accessible @ http:\\\\"};
uint8_t txtErrorInit[] = {"-------- ERROR INITIALIZING HARDWARE --------"};
uint8_t * txtIPAddrItoA;
void iommUnlock (void);
void iommLock (void);
void iommMuxEnableMdio (void);
void iommMuxEnableRmii (void);
void iommMuxEnableMii (void);
void IntMasterIRQEnable (void);
void smallDelay (void);
void sciDisplayText (sciBASE_t *sci, uint8_t *text,uint32_t length);
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
void smallDelay(void) {
static volatile unsigned int delayval;
delayval = 10000; // 100000 are about 10ms
while(delayval--);
}
extern hdkif_t hdkif_data[1];
pbuf_t pack[5];
static uint8 data[5][100];
uint32 size1 = 470,size2=94;
extern uint8 emacAddress[6U];
void create_packet()
{
int i,j;
for(i=0;i<5;i++)
{
pack[i].tot_len = size1;
pack[i].len = size2;
for(j=0;j<6;j++)
{
data[i][j] = 0xffu;
}
for(j=0;j<6;j++)
{
data[i][j+6]= emacAddress[j];
}
data[i][12] = 0;
data[i][13] = 80;
for(j=0;j<80;j++)
{
data[i][j+14] = i+5;
}
pack[i].payload = &data[i][0];
if(i!=4)
pack[i].next = &pack[i+1];
}
pack[4].next= NULL;
}
/* USER CODE END */
void EMAC_LwIP_Main (uint8_t * macAddress)
{
unsigned int ipAddr;
uint8_t testChar;
struct in_addr devIPAddress;
//iommUnlock();
//iommMuxEnableMdio();
//iommMuxEnableMii();
//iommLock();
sciInit();
/* Enable the interrupt generation in CPSR register */
IntMasterIRQEnable();
_enable_FIQ();
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
sciDisplayText(sciREGx, txtTitle, sizeof(txtTitle));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
sciDisplayText(sciREGx, txtTI, sizeof(txtTI));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
#ifdef __little_endian__
// sciDisplayText(sciREGx, txtLittleEndian, sizeof(txtLittleEndian));
// sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
#else
// sciDisplayText(sciREGx, txtBigEndian, sizeof(txtBigEndian));
// sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
#endif
/* Initialze the lwIP library, using DHCP.*/
sciDisplayText(sciREGx, txtEnetInit, sizeof(txtEnetInit));
// ipAddr = lwIPInit(0, macAddress, 0,0, 0, IPADDR_USE_DHCP);
/* Uncomment the following if you'd like to assign a static IP address. Change address as required, and uncomment the previous statement. */
uint8 ip_addr[4] = { 192, 168, 2, 44 };
uint8 netmask[4] = { 255, 255, 255, 0 };
uint8 gateway[4] = { 192, 168, 2, 254 };
ipAddr = lwIPInit(0, macAddress,
*((uint32_t *)ip_addr),
*((uint32_t *)netmask),
*((uint32_t *)gateway),
IPADDR_USE_STATIC);
sciDisplayText(sciREGx, (uint8_t*)"..DONE", sizeof("..DONE"));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
if (0 == ipAddr) {
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
sciDisplayText(sciREGx, txtErrorInit, sizeof(txtErrorInit));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
} else {
/* Convert IP Address to string */
devIPAddress.s_addr = ipAddr;
txtIPAddrItoA = (uint8_t *)inet_ntoa(devIPAddress);
LocatorConfig(macAddress, "HDK enet_lwip");
/* Initialize the sample httpd server. */
sciDisplayText(sciREGx, (uint8_t*)"Starting Web Server", sizeof("Starting Web Server"));
httpd_init();
sciDisplayText(sciREGx, (uint8_t*)"..DONE", sizeof("..DONE"));
sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
/* Loop forever. All the work is done in interrupt handlers. */
while(1)
{
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//sciDisplayText(sciREGx, txtTitle, sizeof(txtTitle));
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//sciDisplayText(sciREGx, txtTI, sizeof(txtTI));
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//#ifdef __little_endian__
//sciDisplayText(sciREGx, txtLittleEndian, sizeof(txtLittleEndian));
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//#else
//sciDisplayText(sciREGx, txtBigEndian, sizeof(txtBigEndian));
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//#endif
//sciDisplayText(sciREGx, txtIPAddrTxt, sizeof(txtIPAddrTxt));
//sciDisplayText(sciREGx, txtIPAddrItoA, 16);
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
//sciDisplayText(sciREGx, txtNote1, sizeof(txtNote1));
//sciDisplayText(sciREGx, txtIPAddrItoA, 16);
//sciDisplayText(sciREGx, txtCRLF, sizeof(txtCRLF));
/* Before printing the next set, wait for a character on the terminal */
//sciReceive(sciREGx, 1, &testChar);
create_packet();
EMACTransmit(&hdkif_data[0], &pack[0]);
}
}
}
void iommUnlock(void) {
/*Unlock the IOMM Register*/
*(int *) 0xFFFFEA38 = 0x83E70B13; /* kicker 0 register, unlock CPU write access to PINMMR registers */
*(int *) 0xFFFFEA3C = 0x95A4F1E0; /* kicker 1 register, */
}
void iommLock(void) {
/*lock the IOMM Register*/
*(int *) 0xFFFFEA38 = 0x00000000; /* kicker 0 register, lock CPU write access to PINMMR registers */
*(int *) 0xFFFFEA3C = 0x00000000; /* kicker 1 register, */
}
void iommMuxEnableMdio(void) {
*(int *) 0xFFFFEB2C = 0x00000400;
*(int *) 0xFFFFEB30 = 0x00000400;
}
void iommMuxEnableRmii(void) {
*(int *) 0xFFFFEB38 = 0x02010204;//P10 //RMIIRXER
*(int *) 0xFFFFEB3C = 0x08020101;//P11 //RMII_RXD0
*(int *) 0xFFFFEB40 = 0x01010204;//P12 //RMII RXD1
*(int *) 0xFFFFEB54 = 0x02040200;//P17 //RMII_RMCRSDV
*(int *) 0xFFFFEB44 = 0x01080808;//P13 //RMII_TXEN , RMII_TX_D1 ,RMII_TX_D0
*(int *) 0xFFFFEB48 = 0x01010401;//P14; //RMII_REFCLK
}
void iommMuxEnableMii(void) {
*(int *) 0xFFFFEB38 &= 0xFFFFFF00; //P10[1] //Mux 10 Rx_ER
*(int *) 0xFFFFEB38 |= (1 << 1); //P10[1] //Mux 10 Rx_ER
*(int *) 0xFFFFEB3C &= 0x00FFFFFF; //P11[26] //Mux 11 Rx[0]
*(int *) 0xFFFFEB3C |= (1 << 26); //P11[26] //Mux 11 Rx[0]
*(int *) 0xFFFFEB40 &= 0x0000FF00;//P12[1,18,26] //Mux 12 Rx[3],Rx[2],Rx[1]
*(int *) 0xFFFFEB40 |= ((1<<26) | (1<<18) | (1<<1));//P12[1,18,26] //Mux 12 Rx[3],Rx[2],Rx[1]
*(int *) 0xFFFFEB44 &= 0x00000000;//P13[2, 10, 26,18] //Mux 13 Tx[2],TxEn,Tx[1],Tx[0]
*(int *) 0xFFFFEB44 |= ((1<<26)|(1<<18)|(1<<10)|(1<<2)); //P13[2, 10, 26,18] //Mux 13 Tx[2],TxEn,Tx[1],Tx[0]
*(int *) 0xFFFFEB48 &= 0xFFFF0000; //P14[9,2,11] //Mux 14 Tx[3],RxClk
*(int *) 0xFFFFEB48 |= ((1<<9)|(1<<2)); //P14[9,2] //Mux 14 Tx[3],RxClk
*(int *) 0xFFFFEB54 &= 0xFF00FF00; //P17[17,1,3] //Mux 17 CRS,TxClk
*(int *) 0xFFFFEB54 |= ((1<<17)|(1<<1)); //P17[17,1] //Mux 17 CRS,TxClk
*(int *) 0xFFFFEB5C &= 0xFFFF00FF; //P19[9] //Mux 19 RxDV
*(int *) 0xFFFFEB5C |= (1<<9); //P19[9] //Mux 19 RxDV
*(int *) 0xFFFFEB60 &= 0xFF00FFFF; //P20[18] //Mux 20 COL
*(int *) 0xFFFFEB60 |= (1<<18); //P20[18] //Mux 20 COL
*(int *) 0xFFFFEB84 &= 0x00FFFFFF;//P29[24] //Mux 29 MII Select pin (24 bit - 0(MII),1(RMII))
*(int *) 0xFFFFEB84 |= (0<<24); //P29[24] //Mux 29 MII Select pin (24 bit - 0(MII),1(RMII))
}
/*
** Interrupt Handler for Core 0 Receive interrupt
*/
volatile int countEMACCore0RxIsr = 0;
#pragma INTERRUPT(EMACCore0RxIsr, IRQ)
void EMACCore0RxIsr(void)
{
countEMACCore0RxIsr++;
lwIPRxIntHandler(0);
}
/*
** Interrupt Handler for Core 0 Transmit interrupt
*/
volatile int countEMACCore0TxIsr = 0;
#pragma INTERRUPT(EMACCore0TxIsr, IRQ)
void EMACCore0TxIsr(void)
{
countEMACCore0TxIsr++;
lwIPTxIntHandler(0);
}
void IntMasterIRQEnable(void)
{
_enable_IRQ();
return;
}
void IntMasterIRQDisable(void)
{
_disable_IRQ();
return;
}
unsigned int IntMasterStatusGet(void)
{
return (0xC0 & _get_CPSR());
}
void sciDisplayText(sciBASE_t *sci, uint8_t *text,uint32_t length)
{
while(length--)
{
while ((sci->FLR & 0x4) == 4); /* wait until busy */
sciSendByte(sci,*text++); /* send out text */
};
}
/* sci notification (Not used but must be provided) */
void sciNotification(sciBASE_t *sci, uint32_t flags)
{
return;
}