Other Parts Discussed in Thread: SM470R1B1M-HT
We are using TMS470-HT / SM470R1B1M-HT (HT implies high temperature) which is ARM7TDMI based core for our application as this works at high temperatures. I understand that this controller does not have ETM (Embedded Trace Macrocell) on it. After checking with TI Technical team, it sounded like there could be a flavor of this controller which has ETM on it. I need a controller which would operate at high temperature and has ETM on it so that I can log the trace of events and the code execution flow.
Is there any revision of this controller that has ETM on it? If not then is there any other part which would operate at high temperature and has ETM on it?