Hello,
I am working with TMS570LS31x/21x. In spnu499b.pdf I can find the information:
a) Page 1718, Table 32-1
According to this table "Group 1 Channel 40" can not be set with a stuck at 0 Test.
b) Page 1721, Table 32-3. EFC Boundary Register (EFCBOUND) Field Descriptions
Bit 20 (EFC Single Bit Error) : This bit drives the single bit error signal when bit 16 (Single bit Error OE) is high.
This signal is attached to ESM error Group 1, Channel 40.
-----------------------------------------------------------------------
According to b) is would look like performing a stuck-at-zero test with bit 16 and 20 in register EFCBOUND would set ESM group 1 channel 40 but this is in contradiction with a) (also I have checked that ESM group 1 channel 40 is not set)
1) What is wrong in spnu499b.pdf? or, am I doing a wrong interpretation?
2) Is there any way of testing ESM group 1 channel 40? (I mean a test that will set this ESM flag).
Thanks,
Francis.