This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting NAND flash MT29F4G16ABADAWP to RM48L952ZWT and ETM capabilities

Hello,

We are looking to connect a 4Gbit NAND flash MT29F4G16ABADAWP to RM48L952ZWT.  Can you confirm the following connections are needed?

·         CLE à EMIF_ADDR[7]   or one GPIO pin

·         ALE à EMIF_ADDR[6]   or one GPIO pin
·         WE# à EMIF_nWE
·         RE# à EMIF_nOE
·         CE# à EMIF_ADDR[8] or one GPIO pin
·         R/B# à one GPIO pin
·         I/O[7:0] à EMIF_DATA[7:0]
·         WP# à Customer’s decision to use it
 
Questions:
1) Is the above connections appropriate to connect to the NAND flash?
2) Is there a scenario we need to use EMIF_nCS[0]? vs using the NAND's CE#?
3) With the configuration above, it appears ETMDATA[11:8] pins will not conflict with EMIF pins EMIF_ADDR[5:2].  Will we then safely have 12 data pins dedicated for ETM?
 
Thanks.
Ubaid