Other Parts Discussed in Thread: EK-TM4C1294XL
I am communicating with an I2C peripheral using an EK-TM4C1294XL. I modified the existing I2C example. The peripheral understands the following protocol: START [address] ACK [reg addr] ACK [reg val] ACK STOP, where the ACKs are generated by the peripheral, and the rest by the Tiva master.
I observe two different scenarios intermittently - proper and erroneous, and I am not able to understand why the erroneous scenario occurs.
Here is my code in main() (excuse formatting):
volatile uint32_t ui32Loop, ui32clock;
uint32_t pui32DataTx[NUM_I2C_DATA], i2c_cmd[NUM_I2C_DATA];
uint32_t ui32Index;
uint8_t err;
ui32clock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_GPIOPinConfigure(GPIO_PB3_I2C0SDA);
MAP_GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
MAP_GPIOPinConfigure(GPIO_PB2_I2C0SCL);
MAP_GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
MAP_I2CMasterInitExpClk(I2C0_BASE, ui32clock, false);
MAP_I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false); // initiate Write operation
// delay a bit
for(ui32Loop = 0; ui32Loop < 8000000; ui32Loop++)
{
}
//
// Initalize the data to send.
//
pui32DataTx[0] = 0x00; // ISL23318 wiper register - holds current wiper position
pui32DataTx[1] = 0x40; // current wiper position to set
i2c_cmd[0] = I2C_MASTER_CMD_BURST_SEND_START;
i2c_cmd[1] = I2C_MASTER_CMD_BURST_SEND_FINISH;
ui32clock = 0;
while(1)
{
ui32Index = 0;
ui32clock++;
pui32DataTx[1] = (0x40)*(ui32clock%3);
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
MAP_I2CMasterDataPut(I2C0_BASE, pui32DataTx[ui32Index]);
MAP_I2CMasterControl(I2C0_BASE, i2c_cmd[ui32Index]);
while(MAP_I2CMasterBusy(I2C0_BASE))
{
UARTprintf(".");
}
err = MAP_I2CMasterErr(I2C0_BASE);
if (err != I2C_MASTER_ERR_NONE)
UARTprintf("error: %d\n", err);
}
UARTprintf(" Complete\n");
for(ui32Loop = 0; ui32Loop < 10000000; ui32Loop++)
{
}
}
Here are the two different pictures I get without any apparent cause for why one is received rather than the other:
In the first case, the first data byte (reg addr) is nowhere to be seen! In the second scenario, I can verify that the transfer is complete and the peripheral responds properly, but why the delay between the 2-nd and 3-rd data bytes?