Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
hi ti,
i have some queries regarding tms570 controller clock frequency.
for tms570lc4357 it is mentioned that crystal frequency range is 5-20 MHz and maximum frequency that can be achieved through PLL is 300MHz.
1. what is the minimum crystal frequency required to achieve 300MHz?
2. if 5MHz crystal is used what is the maximum frequency that can be achieved?
3. in HDK 16MHz crystal is used. Is that the recommended crystal osc freq? if not what all can be used??
4. if 300MHz can be achieved using 16MHz and 20MHz, what is the difference between both? for example in terms of current or power consumption.
5. usually we will be using maximum frequency(300MHz). if we use max freq, whether recommended baud rates for
--> flexray-1.25Mbps, 2.5Mbps, 5Mbps, 10Mbps
--> ethernet - 10Mbps,100Mbps
-->CAN - 125Kbps, 250Kbps, 500Kbps, 1Mbps
--> SCI - 9600bps, 115200bps can be achieved with 0% tolerance?
if there is any reference site or any files pls let me know.
thanks in advance