Other Parts Discussed in Thread: RM57L843, RM48L952, TPS65381-Q1
Hi,
We would like to know if it is possible use single core Cortex-R in Hercules.
One of customer's application needs processor with Speed >220MHz(300DMIPS) and
inbuilt Flash(2 to 4MB). Sitara(AM335x) would be High spec and TIVA C is low spec,
so we believe the only available solution is Hercules.
1. As this is not a Safety related application, can we use only one core in this MCU?
2. And the application needs external 16MB of SRAM with ECC...
Does RM57L843's EMIF interface support external SRAM with ECC?
Best Regards
Kummi