Other Parts Discussed in Thread: HALCOGEN, RM48L952
Hello,
We are using the TI Hercules RM48L952ZWT. We are using HalCoGen to generate our drivers.
1- Where can we look up the base memory address of the board's USB Host Controller that was generated by HalCogen (which file)? When we looked in the HalCoGen User Guide, it does not specify detailed memory map of where the USB Host Controller base address.
2. Does the RM48L952 have a dedicated memory for the USB Host Controller on the Hercules Board? If so where can we find its base address and size?
3. Does the USB Host Controller have direct access to all of the system memory on the Hercules Board?
4. Is there a maximum length of the send/receive buffers for the USB Host Controller integrated on the RM48L952
Thank you.