Other Parts Discussed in Thread: HALCOGEN, TMS570LS1224
I have used the HALCoGen FEE example example_TI_Fee_Write_Read .
I have a question about reading from memory:
The example creates an array of 100 values and writes it to flash memory using TI's F021 Flash API.
Half way the example, it reads the values back into RAM.
I seem to only get 8 values back from the 100 values that were written into Flash.
I used the example from HalCoGen - > Help -> Examples -> example_TI_Fee_Write_Read
(followed the instructions in HALCoGen help, and took source from HALCoGen's help folder)
I've tried this on two Hercules controllers; the TMS570LS04x and RM46x.
This is the result I get in the 'read_data' variable:
8 values are read back as expected, but the previous lines of code wrote 100 values.
The source code can be viewed by starting HALCoGen, go to Help -> Help Topics
Navigate to: Examples -> example_TI_Fee_Write_Read.c
One of my fellow e2e mebers, Martin Valencia, detected the issue, and I can replicate it on two controllers.
Very likely, we understand the fee driver and Flash API wrong. It would be great if you could point us to the right direction.