Other Parts Discussed in Thread: TM4C123GH6PM, ISO1050, SN65HVD1050
I use two pieces of tm4c123gxl. Even with 2 mcp2551 & 2 120 ohms resistors to make a can bus system. I use sample programs, simpletx & simplerx, provided by TI. When run the project, a status interrupt occurred with status numbers of 4 & 5, which means that a 0 or 1 is on the can bus too long time. Anybody knows the reason for that?