I cannot connect to the board. I am using CCS5.5.0.
I have tried reinstalling CCS, but no luck.
The error when i try to connect is:
IcePick: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.1.232.0)
I can only assume i need an FTDI driver for the board? When i plug in the USB, i see two "USB Composite Device" entries in device manager. Windows 7 x64.