This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SW-DK-LM3S9B96-V6075 software download

Hi 

i am working on a 4.5 inch kentec LCD interfacing to TIVA and i have found driver file for this but main code written in SW-DK-LM3S9B96-V6075   version is 6075 ,but i am not able to download this version so please share me the V6075 link to download the software.

Regards

Nandish

  • Hello Nandish

    All LM3S device were bundled in the final StellarisWare release 9453. We are not maintaining any older release.

    Regards
    Amit
  • Hi Amit

    thanks for the reply,but when i was trying to interface 4.5 inch kentec LCD they have given the example driver code but for remaining code they mentioned its developed in stellarisware V6705 . can you please get me the 4.5 inch LCD interfacing code.

    Regards

    Nandish

  • Hello Nandish,

    I am sorry I cannot help you with that.

    Hello Forum.

    If anyone has the v6705 release, then could you please share it with nandish

    Much Appreciated...
    Thanks
    Amit
  • Nandish H S said:
    trying to interface 4.5 inch kentec LCD

    I'm in the display biz - suspect you mean (instead) 4.3" LCD. (w/480x272 pixel resolution - although latest/greatest have advanced to 800x480)

    Now somewhere - our small firm (likely) has StellarisWare 6705 - but I can recall NO special code (confined) "only" w/in that version of StellarisWare.  Do you believe that it makes sense for predecessor (or current) vendor to create a special code module - integrate it w/in Ver 6705 - and then "yank it?"  (doubtful - don't you agree?)  And - in the unlikely event that the code was a "one hit wonder" - does not that signal that faults were found - thus it's withdrawal from all future versions?

    Might you double check - and present their writing which suggests "driver code" is limited to just this - single version of StellarisWare?  Makes very little (i.e. NO) sense - believe something has been lost in translation...