This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva C TM4C129 I2C Master implementation questions



Hello e2e folks-

I'm working on a simple I2C network with just two members, a Tiva C TM4C1294 launchpad and an arduino Uno. The Uno is acting as a slave and when prompted should return 4 2-byte variable values, and I think I have that working well enough.

So my problem is with the Tiva, I don't quite get how I2C works on this board, how to initialize it properly and request/receive values from slave devices.

I found this example code here-

#define ACCEL_SLAVE_ADDR 0x1D
#define XOUT8 0x06
#define YOUT8 0x07
#define ZOUT8 0x08
 
uint8_t ReadAccel(uint8_t reg)
{
    uint8_t accelData =  I2CReceive(ACCEL_SLAVE_ADDR, reg);
 
    return accelData;
}
 
void main(void)
{
    // Set the clocking to run directly from the external crystal/oscillator.
    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_PLL | SYSCTL_OSC_INT | SYSCTL_XTAL_16MHZ);
 
    //initialize I2C module 0
    InitI2C0();
 
    uint8_t Ax, Ay, Az;
 
    Ax = ReadAccel(XOUT8);
    Ay = ReadAccel(YOUT8);
    Az = ReadAccel(ZOUT8);
 
    while(1){};
}

I see that it's setting XOUT8, YOUT8, and ZOUT8 to read values from I2C, and sending seemingly arbitrary numbers as the "reg" argument in the ReadAccel function. I don't understand how that correlates to requesting the data from those registers and what exactly accelData has as a value after reading in bytes. Is it the last value that the slave sent?

In case I'm making things more difficult for myself, I'm just trying to send 4 2-byte variables from the arduino slave to the tiva master, if there's an easy way to do this I'd love any suggestions you guys might have.

Thank you

Garrett

  • Hello Garrett

    May be a simple example code like the following will help you understand the I2C Master

    C:\ti\TivaWare_C_Series-2.1.0.12573\examples\peripherals\i2c\master_slave_loopback.c

    Do remember that it loopback from the same master to slave, so if you do not consider the slave portion of the code then this code is the low level driver that ReadAccel will come down to.

    Regards
    Amit