I had ordered Tiva™ C Series TM4C123G LaunchPad for the TIIC-India Design Contest. I installed all the drivers present on the website. But the board's power LED(green) is glowing dimly and the board is getting very hot within seconds after connecting it to the USB port of the laptop. Moreover, the board is not getting detected and no RGB LED code is working, which, as per the manual, should have come pre-loaded in the board.
Can I get the board replaced ? It is the main component of my project so I need it for carrying it out.