Other Parts Discussed in Thread: TM4C1230C3PM
I am using tm4c1230c3pm platform and coding with Keil uVision5.
I want to cast the uint32_t into float with 3 significant figures.
I tried casting so many times referring to other suggestions in the web with channel 4 output in my code, but it gave me ERROR every single time.
help me please~~~~
any suggestions would be appreciated!!
here's my entire codes
#include <stdio.h>
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc\hw_uart.h"
#include "inc/hw_gpio.h"
#include "inc\hw_ints.h"
#include "driverlib\pin_map.h"
#include "driverlib\rom.h"
#include "driverlib\rom_map.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/uart.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "utils/uartstdio.h"
#include "utils/softssi.h"
#define DATA_LEN 16
uint32_t g_ui32SendData[DATA_LEN], g_ui32RcvData[DATA_LEN];
void readdata(void);
int nullVal = 0;
uint32_t adcdata[4];
void delay(volatile unsigned long ulDelay){
ROM_SysCtlDelay((ROM_SysCtlClockGet() / (1000*3)) * ulDelay);
}
void ConfigureUART(void){
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
UARTStdioConfig(0, 115200, 16000000);
}
void ConfigureSSI(void){
ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_INT | SYSCTL_MAIN_OSC_DIS);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_GPIOPinConfigure(GPIO_PD0_SSI1CLK);
ROM_GPIOPinConfigure(GPIO_PD1_SSI1FSS);
ROM_GPIOPinConfigure(GPIO_PD2_SSI1RX);
ROM_GPIOPinConfigure(GPIO_PD3_SSI1TX);
ROM_GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1| GPIO_PIN_2| GPIO_PIN_3);
ROM_SSIClockSourceSet(SSI1_BASE, SSI_CLOCK_PIOSC);
ROM_SSIConfigSetExpClk(SSI1_BASE, ROM_SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
SSI_MODE_MASTER, 115200, 16);
ROM_SSIEnable(SSI1_BASE);
}
float uintToFloat (uint32_t intVal){
uint32_t temp = intVal;
float floatVal = temp;
return floatVal;
}
int main(void){
volatile float rxData;
ROM_FPULazyStackingEnable();
ConfigureSSI();
ConfigureUART();
// CONVST
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_5);
while(1){
unsigned char i;
ROM_GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5, 0);
ROM_GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5, GPIO_PIN_5);
//CS
ROM_GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_1, 0);
while(ROM_SSIBusy(SSI1_BASE));
while(ROM_SSIDataGetNonBlocking(SSI1_BASE, &g_ui32RcvData[0]));
SSIDataPut(SSI1_BASE, nullVal);
SSIDataGet(SSI1_BASE, &adcdata[0]);
UARTprintf(" \nreceived %d", adcdata[0]);
SSIDataPut(SSI1_BASE, nullVal);
SSIDataGet(SSI1_BASE, &adcdata[1]);
UARTprintf(" \nreceived %d", adcdata[1]);
SSIDataPut(SSI1_BASE, nullVal);
SSIDataGet(SSI1_BASE, &adcdata[2]);
UARTprintf(" \nreceived %d", adcdata[2]);
SSIDataPut(SSI1_BASE, nullVal);
SSIDataGet(SSI1_BASE, &adcdata[3]);
rxData = uintToFloat(adcdata[3]);
UARTprintf(" \nreceived %.3f", rxData);
UARTprintf("\nCh1 voltage 1= %d Volts", adcdata[0]/3266); // *((float*)&adcdata[0])/3266)
UARTprintf("\nCh2 voltage 2= %d Volts", adcdata[1]/3266);
UARTprintf("\nCh3 voltage 3= %d Volts", adcdata[2]/3266);
UARTprintf("\nCh4 voltage 4= %.3f Volts", (float) rxData/3266.0);
while(ROM_SSIBusy(SSI1_BASE));
delay(1000);
}
}
OUTPUT