Hi Friends
i'm uising ccs 5.5. I would like to open(Not IMPORTING) an existing project. How can I do that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Friends
i'm uising ccs 5.5. I would like to open(Not IMPORTING) an existing project. How can I do that?
Hello Amit
If i import an existing project then ccs shows an error that same project already exist in workspace. And it is obvious because that project already exist in that workspace. Actually in past i deleted that project from the workspace in ccs without deleting it from its original location. Now how can i open this project?
Hello Amit
I''m not able to understand
1. in-situ compilation.
2. it will run the code wherever the project is without importing it. How can i run a project without importing it?
Hello Amit
I think, it will be similar to automatically linking project which is found while importing projects.
Hello Amit
Thanks For Quick Reply.
Can you please explain me this different?