Other Parts Discussed in Thread: TMS570LC4357, TMS570LS20216
Hello Team TI
I use TMS570LC4357 and TMS570LS20216. I have the following questions regarding FlexRay Peripheral available in these MCUs.
1) From the Protocol Spec v2.1, the communication cycle time ranges from 10us to 16ms. Does both these controllers support 10us cycle time. If it does, please explain with justification. If there is any use-case example that justifies this point, it would be of great help.
2) Does any safety controllers of TI support FlexRay Protocol v3.0.1 and ISO 17458 ? If yes, kindly list them.
Thanks in advance !