Other Parts Discussed in Thread: CC3200, CC3100, TM4C1294NCPDT
Hi,
I want to connect and communicate a Tiva TM4C1294 Connected LaunchPad with a CC3200. Please give a complete description of how to do that, and provide documentation. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC3200, CC3100, TM4C1294NCPDT
Hi,
I want to connect and communicate a Tiva TM4C1294 Connected LaunchPad with a CC3200. Please give a complete description of how to do that, and provide documentation. Thanks!
Hi Fernando,
I agree completely with Markel, using the CC3100 boosterpack with the TM4C1294 launchad would be a much better idea
Uhmmmm.. Again Imperative form.... I am thinking about this, someone agree as appropriate answer to bad request form? :D I wish a pleasant enjoy. (P.S. this got translated to many languages)
Forever I forgot original post: which one of multichannel are on both board and processor is/are to be selected for communication and to do what and why?
No details no possible answers.
[Edit changed some word and splitted lines]
And about imperative, we are payd for? So why someone has to do that?
Fernando, I suggest learn something about different language use verb and courtesy:
--->> I want ---- give a complete description...
Sound too bad on English and I fear you literally translated from your native language. Learn about I wish, please and full courtesy form. AVOID imperative.. So you MUST say sorry for that also if I understand why but you MUST avoid that.
suggested phrase :
--- Please accept my apologizes about worst usage of my little English. ----
I am not native too and sometimes I wrote in unreadable form, but when happen is not question of foreign It can appear also on native too. Read again before post, preview of forum is no more here. :( [Edit : aafter reading the post I got back to repair disaster ;) ]
Hi Luis, I like you liked it, I hope after edit, before was possible to feel as worst than imperative...
I wish have again post preview but I fear it is no more possible.
Hi Fernando,
It would be better to further ask help at the Simplelink Wifi CC31xx/CC32xx forum, if you want to connect Tiva Connected Launchpad and CC3100 Booster Pack. There are some people who frequent the forum who might be able to help you, including TI Engineers.
Also it would help you a lot if you go through the related technical documents for CC3100 and CC3200.
- kel
Fernando Sanchez1 said:Is there a better way to approach the problem than using the steps suggested in the post above.
Hi Fernando, I see you accepted suggestion, apologizes where not needed, it was just a suggestion I appreciate it was useful for you BUT you are still asking something still not documented.
What communication type you wish to implement between board? SPI parallel mode can be the fastest but to do what? Maybe some other solution are appliable.
Forever on post like your the worst trouble is to understand what the poster is asking us. Can you try explain more? Use short phrases it is forever better.